Hi all,
We are using imx_"3.14.38_6qp_ga yocto fido" bsp in our custom board. uboot version 2015.04.
In this after enabling usb in uboot when we boot the below error print is appearing.
""## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
EHCI failed to shut down host controller.
Using Device Tree in place at 18000000, end 1801017d"
Could anybody tell me why this print is appearing and any solution for this issue.
Thanks in advance.
Regards,
Yashavantha
Solved! Go to Solution.
Hi yashavantha
seems this fixes below patch
[U-Boot] [PATCH 1/3] arm: mx6: cm-fx6: force host mode on usb controller
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi yashavantha
seems this fixes below patch
[U-Boot] [PATCH 1/3] arm: mx6: cm-fx6: force host mode on usb controller
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi yashavantha
are u able to fix the issue using the patch..