Hi all,
I dont know what some Uboot cmd can be applied to on MX6DL Uboot 2014.04,such as
loop - infinite loop on address range
This cmd will read the memory addr range as fast as possible,it's a infinite loop, but I dont know if it is meaningful,some articles say it can used for ddr test, I cannot understand it.
help me,Thank you ~
Hi Tony,
About the ddr test you can refer to i.MX6/7 DDR Stress Test Tool V2.40 .
Have a great day,
Dan
Hi tony,
Which version BSP are you using?
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
uboot 2014.04
kernel Linux version 3.10.53
Android l5.0.0_1.0.0-ga
sorry I dont know whats your meaning about bsp version, hope the above can help you.
Now my problem is unsolved.
Thank you~
Hi tony,
The Android l5.0.0_1.0.0-ga is your BSP version. I will confirm your question for you. Here can you tell me the board you are using is the board you buy from our company or you designed it yourself?
Best Regards
Dan
Hi, wang
Designed by ourselves.