series capacitor for the signal WDOG_B on the Buffer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

series capacitor for the signal WDOG_B on the Buffer

550 Views
prev
Contributor II

Hi

Can you explain the use of series capacitor for the signal WDOG_B on the Buffer.

As the series capacitor blocks DC and then the logic level is asserted.

pastedImage_0.png

Regards

Ravanth

Labels (4)
Tags (1)
0 Kudos
Reply
1 Reply

474 Views
Pavel
NXP Employee
NXP Employee

Look at the following documents:

https://www.ece.cmu.edu/~ee100/docs/Chapter8.pdf

and

http://electronics.stackexchange.com/questions/158015/how-to-turn-continuous-signal-into-a-short-pul...


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply