Hello together,
This is the first time I bring up so may imx6 hardwares for my customer . My hardware has:
Below is my plan for bringing up:
This is my questions related to the steps to bring up hardware:
Thanks,
Tan
Hello,
You may check memory using the DDR stress tool, which needs only
USB OTG port of the i.MX6 : the result is sent to PC through USB
and displays in the log window. Also, JTAG-loadable version is located
there. No UART is needed.
i.MX6/7 DDR Stress Test Tool V2.30
For memory initialization, please refer to the following :
As for eMMC support, please refer to the following :
i.MX6: Accessing boot/user partitions on eMMC
how to change emmc linux driver
Customer Borqs(ChinaTSP) encounter some issues when implement “raw eMMC driver” in i.MX6 platform.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri,
Because my board don't have USB OTG port but UART 1 and JTAG connector. So could you please show me how to get the result when calibrating RAM?
I am looking forward to your help!!
Thanks,
Tan
Hi,
the mentioned stress tool has JTAG and UART based release :
Regards,
Yuri.
Our hardware doesn't have USB OTG port. How can I get the result when checking RAM?
I am looking forward your respond!!!
Thanks,
Tan