Hi,
I want to check SI with IBIS model for MCIMX6S7CVM08AC(industrial grade) but
I could find only 2 .ibs in the zip file as following.
i.MX 6DualLIte and i.MX 6Solo IBIS File (REV 1.4.)
https://www.freescale.com/webapp/Download?colCode=IMX6_DL_S_IBISmx6sdl_21x21_autmtv_v1_4.ibs
mx6sdl_21x21_consmr_v1_4.ibs
(Q) Which one is for the industrial grade?
Anyone can help me? I guess "consmr" represents both Consumer and Industrial.
Thanks.
Solved! Go to Solution.
Hi torus1000
please use the automotive version for industrial i.MX6 parts.
Below is Community discussion link about the isue.
Which type IBIS model should I select using with industrial i.MX6DL ?
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi torus1000
please use the automotive version for industrial i.MX6 parts.
Below is Community discussion link about the isue.
Which type IBIS model should I select using with industrial i.MX6DL ?
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------