Which IBIS file is for the industrial grade of i.MX6S?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which IBIS file is for the industrial grade of i.MX6S?

Jump to solution
797 Views
torus1000
Contributor V

Hi,

I want to check SI with IBIS model for MCIMX6S7CVM08AC(industrial grade) but
I could find only 2 .ibs in the zip file as following.

i.MX 6DualLIte and i.MX 6Solo IBIS File (REV 1.4.)
https://www.freescale.com/webapp/Download?colCode=IMX6_DL_S_IBIS

     mx6sdl_21x21_autmtv_v1_4.ibs
     mx6sdl_21x21_consmr_v1_4.ibs

(Q) Which one is for the industrial grade?

Anyone can help me? I guess "consmr" represents both Consumer and Industrial.

Thanks.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
640 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

please use the automotive version for industrial i.MX6 parts.

Below is Community discussion link about the isue.

Which type IBIS model should I select using with industrial i.MX6DL ?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
641 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

please use the automotive version for industrial i.MX6 parts.

Below is Community discussion link about the isue.

Which type IBIS model should I select using with industrial i.MX6DL ?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply