Hello,
Can anyone please tell me what is the maximum size of external flash that can be connected to K70 and also the source from where this info was taken
Thanks
Sudeep
Hi Sudeep,
as you can see in the Reference Manual you have the option to use Multiplexed 32-bit address and 32-bit data. Therefore you can address 2^32 bytes.
Best regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------