Hi jie jia,
You can modify the logo.c file in linux driver. Replace the display penguins when kernel boot up with your logo picture. In the linux BSP, the path of logo.c file is /linux-3.0.35/drivers/video/logo/logo.c, if you are using the linux-3.0.35 vesion BSP.
Here you have to make sure the Resolution are the same with the penguins on display.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi jie jia,
You can modify the logo.c file in linux driver. Replace the display penguins when kernel boot up with your logo picture. In the linux BSP, the path of logo.c file is /linux-3.0.35/drivers/video/logo/logo.c, if you are using the linux-3.0.35 vesion BSP.
Here you have to make sure the Resolution are the same with the penguins on display.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Please read this article about keeping the U-Boot logo while the kernel is booting up:
Regards,
Gary