Hi,
I'm confused with rtl8188usb-wifi configuring in terminal on imx6q with linux-3.14.28.When I use the UI connect manager with lcd,it's easy to connect to the wifi.While removing the lcd and configuring in the terminal ,it's always failed.I modify the "/etc/ wpa_supplicant.conf" and use "wpa_supplicant -B -D wext -i wlan0 -c /etc/wpa_supplicant.conf" cmd,it returns:
Successfully initialized wpa_supplicant | |
rfkill: Cannot open RFKILL controR8188EU: ERROR indicate disassoc | |
l device | |
ioctl[SIOCSIWAP]: Operation not permitted | |
root@imx6qsabresd:~# R8188EU: ERROR assoc success | |
R8188EU: ERROR indicate disassoc | |
IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready | |
R8188EU: ERROR assoc success | |
IPv6: ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready | |
R8188EU: ERROR indicate disassoc | |
R8188EU: ERROR assoc success | |
IPv6: ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready | |
R8188EU: ERROR indicate disassoc | |
R8188EU: ERROR assoc success |
R8188EU: ERROR indicate disassoc
.....
anyone who is familiar with this could help me.
Thanks very much.
It seems using connman tool,I use connmanctl cmd and success to connect to the wifi that I point to
cloud you tell me what ‘s the connmanctl cmd ?