Hi,
I'm confused with rtl8188usb-wifi configuring in terminal on imx6q with linux-3.14.28.When I use the UI connect manager with lcd,it's easy to connect to the wifi.While removing the lcd and configuring in the terminal ,it's always failed.I modify the "/etc/ wpa_supplicant.conf" and use "wpa_supplicant -B -D wext -i wlan0 -c /etc/wpa_supplicant.conf" cmd,it returns:
Successfully initialized wpa_supplicant | |
rfkill: Cannot open RFKILL controR8188EU: ERROR indicate disassoc | |
l device | |
ioctl[SIOCSIWAP]: Operation not permitted | |
root@imx6qsabresd:~# R8188EU: ERROR assoc success | |
R8188EU: ERROR indicate disassoc | |
IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready | |
R8188EU: ERROR assoc success | |
IPv6: ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready | |
R8188EU: ERROR indicate disassoc | |
R8188EU: ERROR assoc success | |
IPv6: ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready | |
R8188EU: ERROR indicate disassoc | |
R8188EU: ERROR assoc success |
R8188EU: ERROR indicate disassoc
.....
anyone who is familiar with this could help me.
Thanks very much.