Has anyone completed a port of the serial profile for USB on the i.Mx51 Babbage or i.Mx53 platform running Gingerbread?
I started this port about 10 months ago then got way-laid on other projects:
Step 1) Porting the support from a new Kernel to the R10 then
step 2) build hooks into Android.
I completed the Kernel update - but there it sits.
If anyone has completed this effort to so a design based on the BBG-Gingerbread or Mx53-Gingerbread platform will support USB to Serial dongle's PLEASE reply to me or to this post. It would be MOST appreciated!
Thanks!
Mike
已解决! 转到解答。
Hi Mike,
In linux kernel, there are some typical parts for USB to Serial converter, such as CP210x , FTDI devices etc, so anyway, haredware design or driver for linux(android) are both no problem, you can select one of them for your solution.
Regards,
Weidong
Hi Mike,
In linux kernel, there are some typical parts for USB to Serial converter, such as CP210x , FTDI devices etc, so anyway, haredware design or driver for linux(android) are both no problem, you can select one of them for your solution.
Regards,
Weidong
Weidong,
Thanks for your reply - yes this is true and I have utilized the FTDI driver for the Kernel portion.
My expectation is that this is only 1/2 of the support needed.
The exposure of this support to Android is where I am missing some pieces.
How/what is needed for Android to recognize this additional support? Typically (for other features I have added) I have found that I need to modify the Android-OS as well.
If you can provide any guidance that would be awesome!
Thanks,
mike