Hi guys,
I'm trying to use DMA for one of the UART's on TWRK65F180M using MQX 4.1
I have already implemented the UART driver using interrupt and it works fine. Now I want to use DMA for that UART for obvious reasons.
I can see a file in the BSP project with the name serl_dma_kuart.c which contains function related to DMA. But I don't see those functions being referenced anywhere else.
Does MQX support DMA for UART's?
Your help is much appreciated. Thank you.
Regards,
Vivek
Hello Vivek,
Please check the below threads
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------