Hi --
I have a custom board with a K64FX512, and CW 10.6. My program just waves some I/O lines up and down. There is one, single bit output, and one, two bit output. No timers, no interrupts, nothing. I have a compiler error that says: "Auto select settings failed because there are no other proper requirements for timing configuration (Counter frequency)" and under Location, it says "TU1/Counter frequency" and under Type it says "Processor Expert Problem". There is a second one that is identical except it says "TU1/Overrun period".
The odd part is that I am not using a timer for anything, and the K64 Reference Manual has no entry for "TU1".
So, what is it, where is it, and how do I get rid of it?
Hello Gary,
Please send your project to me , or i can not understand your problem , thank !
BR
Alice
Hi Alice --
I have it zipped up, but how do I attach it, or send it to you? The "Actions" button says no actions are available.
Hello Gary,
1.
2.
BR
Alice
Yes, I tried that, but mine only says "No actions are available."
In any case, I accidently stumbled across the answer. If you right click on the error message in the Problems window, a list box pops up, and one of the choices is "Open Processor Expert Problem". Double click on that, and the Component Inspector opens up with "TU1" selected.