I'm unable to boot the device. The init process is failing. I'm using the supplied shell script to flash the sdcard.
I'm copying the system partition directly from the out folder.
Just wondering is there an issue with reading the sdcard.
line.360 check_partition:161, name-p mmcblk3: unknown partition table
Added prints in system/core/init process
logs attached.
Original Attachment has been moved to: errMinicomLog.zip
Hi k
it may be recommended to check device tree file if
mmcblk3 is configured properly.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------