sabresd_6dq booting issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sabresd_6dq booting issue

361 Views
kmani
Contributor I

I'm unable to boot the device. The init process is failing. I'm using the supplied shell script to flash the sdcard.

I'm copying the system partition directly from the out folder.

Just wondering is there an issue with reading the sdcard.

line.360 check_partition:161, name-p mmcblk3: unknown partition table

Added prints in system/core/init process

logs attached.

Original Attachment has been moved to: errMinicomLog.zip

Labels (1)
0 Kudos
1 Reply

288 Views
igorpadykov
NXP Employee
NXP Employee

Hi k

it may be recommended to check device tree file if

mmcblk3 is configured properly.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos