the video of I.MX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the video of I.MX6Q

721 Views
123
Contributor I

dear all:

The recommended program of 360-degree surroudview  with I.MX6Q is  to connect  the  tw6865 with PCIE.

Can tw2868 or tw2968 to replace tw6865 ???

(Both of them supports ITU-R BT.656 type time multiplexed output with 54/108MHz)

Labels (1)
0 Kudos
Reply
2 Replies

588 Views
Yuri
NXP Employee
NXP Employee

  Basically it is possible to use any device of 4-in-1 video decoders with

PCI Express. Another question - software compatibility, or corresponding driver presence.

It is needed to apply for manufacturer regarding the driver.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

588 Views
123
Contributor I

Thanks, how about the MIPI CSI2 and BT.656  for 4-in-1 video decoder???

Can I.MX6Q support them?

0 Kudos
Reply