About i.MX6Q PCIe EP/RC Validation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About i.MX6Q PCIe EP/RC Validation

755 Views
mingmingyuan
Contributor III

dear fsl:

board:sambasd

system:linux 3.0.35

i.MX6Q PCIe EP/RC Validation System

I want to use above method for verify my pcie bus. but I have only one sambasd board. So I use a fpga as EP.

sambasd board(RC mode)<------>fpga(EP mode)

but I find pcie.c have define EP_SELF_IO_TEST, this is only used for EP mode.

Now I want to use EP_SELF_IO_TEST in RC mode ,Can you tell me how to change? thanks!

Labels (2)
0 Kudos
Reply
3 Replies

592 Views
igorpadykov
NXP Employee
NXP Employee

Hi mingming

on that link one board is used in RC mode and you can use

its settings

When building RC image, make sure that

        CONFIG_IMX_PCIE=y

        # CONFIG_IMX_PCIE_EP_MODE_IN_EP_RC_SYS is not set

        CONFIG_IMX_PCIE_RC_MODE_IN_EP_RC_SYS=y

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

592 Views
mingmingyuan
Contributor III

dear sir:

Thanks for your help!

I know how to set boart to RC mode.

My problem is how to use EP_SELF_IO_TEST function?

because this function is used by EP mode according pcie.c code. Now I want to use this function in RC mode!

0 Kudos
Reply

592 Views
mingmingyuan
Contributor III

dear sir:

this problem is very important to me.

can you help me? thank you very very much!

0 Kudos
Reply