Hello,
I created a project using KSDK/PE with MQX, 1 task added, 1 event created, but when compiling:
when i go into psp_time.h, and right click PSP_TICK_STRUCT_PTR to open declaration, KDS can find the declaration in the mqx.h.
So it's the problem of compiler settings?
Find my project in attach
Thanks,
Hancheng YANG
Original Attachment has been moved to: 2204_migration_KSDK_PE_d.7z.zip
Hello ,
When use MQX_KSDK, it needn't add the mqx_ksdk component, we only need choose here :
this function is equivalent to MQX_KSDK. There are all the OS the KSDK concluded, we can refer to our need select.
Please see the attachment , it is a project i create on my side , you can try it on your side .
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------