Hi all,
I am doing one real time application project using iMX6sl with yocto linux. I want to enable USB_ETHernet support in kernel configuration. I have enabled this by using make menuconfig. But it is not working.SO, i want to know that Is it possible to use both FEC ( Fast Ethernet Controller) and USB_ETH..? and Should i do disable FEC to use USB_ETH..? Or is any other way to enable USB_ETH support in kernel...?
Hi ANBU
it is possible to use both FEC and USB_ETH.
Please look at attached doc file from imx-test package,
describing USB Gadget Ethernet test, so new device is created:
ifconfig usb0 10.0.0.105
ip addr show usb0
Linux-USB Gadget API Framework
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------