In MAPLE-B3 PUSCH2_EDF, What about "DFT processing of cancelled layers using the eFTPE2" ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In MAPLE-B3 PUSCH2_EDF, What about "DFT processing of cancelled layers using the eFTPE2" ?

2,852 Views
mohamedtaha
Contributor I

As mentioned in the attached document "MAPLE-B3RM_RevE_B4860Rev2_A28.pdf", page 2, DFT processing of cancelled layers can be done using eFTPE2 within PUSCH2_EDF processing chain and this is optional.

pastedImage_0.png

But there isn't any other information in the same document describing how to enable this. Also section 1.4.6 which describe PUSCH2_EDF, doesn't include any information about DFT processing of cancelled layers using the eFTPE2. So, how to enable this feature? is enabling this feature is mentioned in another document?

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,326 Views
lunminliang
NXP Employee
NXP Employee

Hi,

I think this means DFT processing for cancelled layers is optional for PUSCH2_EDF processing flow, which could be implemented by eFTPE2. DFT as function/feature of eTFPE is not necessary to enable.

0 Kudos
Reply

1,326 Views
mohamedtaha
Contributor I

Hi,

Yes, DFT processing for cancelled layers is optional for PUSCH2_EDF processing flow using eFTPE2. But how can I enable this option?

0 Kudos
Reply