Hi, is it possible to use other eink displays with the SABRE Platform for eReaders based on i.MX50? We are using the Eink mobius. Also, how many gpio are available? Thanks
Hi Gal
i.MX50 FSL software supports only panels found on MX508-EVK Based E-Book add-on Board
though other panels also may be supported (sw modifications are needed).
IMXEBOOKDC2 E-BOOK Exp Daghter Card
L2.6.35__11.04_ER_SOURCE : Linux 2.6.35 Source Code Files and documentation 2011.04.
Regarding gpios, there are 6 GPIO modules (each 32bit), please read IMX50RM
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------