Hi, is it possible to use other eink displays with the SABRE Platform for eReaders based on i.MX50? We are using the Eink mobius. Also, how many gpio are available? Thanks

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, is it possible to use other eink displays with the SABRE Platform for eReaders based on i.MX50? We are using the Eink mobius. Also, how many gpio are available? Thanks

1,069 Views
galdolber
Contributor I

Hi, is it possible to use other eink displays with the SABRE Platform for eReaders based on i.MX50? We are using the Eink mobius. Also, how many gpio are available? Thanks

Labels (2)
0 Kudos
Reply
1 Reply

895 Views
igorpadykov
NXP Employee
NXP Employee

Hi Gal

i.MX50 FSL software supports only panels found on MX508-EVK Based E-Book add-on Board

though other panels also may be supported (sw modifications are needed).

IMXEBOOKDC2 E-BOOK Exp Daghter Card

L2.6.35__11.04_ER_SOURCE : Linux 2.6.35 Source Code Files and documentation 2011.04.

Regarding gpios, there are 6 GPIO modules (each 32bit), please read IMX50RM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply