Hi all
I want to know a IPU processing performance of i.MX6Q/D.
Does anyone have IPU's processing performance data per second ?
I don't know whether IPU can process a data without affecting the CPU in my system that have two CSI input(1080p@60) and one display output(1080p).
I'm concerned about a load of CPU when the IPU processing will overflow.
I can't find it in RM in these respects.
For instance, let me talk about Image Converter (IC).
According to the RM, the maximum rate of input from sensor is 200M pixels/sec and output to display is 100M pixels/sec.
However, there is no description about processing time when performing such as Resizing, Color conversion, etc.
So please provide me a IPU's processing performance data per second if you have it.
Best Regards,
ko-hey
Solved! Go to Solution.
Hi ko-hey
I am afraid such IPU's processing performance is not available,
however I would recommend to look at below presentation
(one can ask local FAE to obtain it for any access issues)
FTF-CON-F0119 "A Deep Dive into Image Processing for i.MX 6 Series Applications Processors"
Freescale Technical Sessions Library|Freescale
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi ko-hey
I am afraid such IPU's processing performance is not available,
however I would recommend to look at below presentation
(one can ask local FAE to obtain it for any access issues)
FTF-CON-F0119 "A Deep Dive into Image Processing for i.MX 6 Series Applications Processors"
Freescale Technical Sessions Library|Freescale
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor
Can I provide the PDF to my customer ?
Is that a confidential material ?
Best Regards,
ko-hey
Hi ko-hey
yes it can be shared with customer.
Best regards
igor
Hi Igor
Thank you!
ko-hey