i.MX6Q/D IPU performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q/D IPU performance

Jump to solution
768 Views
ko-hey
Senior Contributor II

Hi all

I want to know a IPU processing performance of i.MX6Q/D.

Does anyone have IPU's processing performance data per second ?

I don't know whether IPU can process a data without affecting the CPU in my system that have two CSI input(1080p@60) and one display output(1080p).

I'm concerned about a load of CPU when the IPU processing will overflow.

I can't find it in RM in these respects.

For instance, let me talk about Image Converter (IC).

According to the RM, the maximum rate of input from sensor is 200M pixels/sec and output to display is 100M pixels/sec.

However, there is no description about processing time when performing such as Resizing, Color conversion, etc.

So please provide me a IPU's processing performance data per second if you have it.

Best Regards,

ko-hey

0 Kudos
1 Solution
576 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

I am afraid such IPU's processing performance is not available,

however I would recommend to look at below presentation

(one can ask local FAE to obtain it for any access issues)

FTF-CON-F0119 "A Deep Dive into Image Processing for i.MX 6 Series Applications Processors"

Freescale Technical Sessions Library|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
4 Replies
577 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

I am afraid such IPU's processing performance is not available,

however I would recommend to look at below presentation

(one can ask local FAE to obtain it for any access issues)

FTF-CON-F0119 "A Deep Dive into Image Processing for i.MX 6 Series Applications Processors"

Freescale Technical Sessions Library|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
576 Views
ko-hey
Senior Contributor II

Hi Igor

Can I provide the PDF to my customer ?

Is that a confidential material ?

Best Regards,

ko-hey

0 Kudos
576 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

yes it can be shared with customer.

Best regards

igor

0 Kudos
576 Views
ko-hey
Senior Contributor II

Hi Igor

Thank you!

ko-hey

0 Kudos