i.MX6SL Power Dissipation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SL Power Dissipation

1,072 Views
tony_l_cai
Contributor III

Hi,Community,

      I want to get some info about i.MX6SL Power Dissipation during Deep sleep and test condition such as the DDR type,size and so on.

      Of cause,other info about i.MX6SL Power Dissipation during different status can be provided, I'm also glad to accept.

      Thank you!

Labels (3)
0 Kudos
Reply
3 Replies

964 Views
igorpadykov
NXP Employee
NXP Employee

Hi 龙

you can find such data in below app note

AN4580 i.MX 6SoloLite Power Consumption Measurement

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

964 Views
tony_l_cai
Contributor III

Thanks igorpadykov

Can you help me to find some info related to the i.MX6SL boot flow especially DDR3L/LPDDR2 Load in the boot flow?

I need some Linux SW knowledge including  DDR3L/LPDDR Load/usage in i.MX6SL.

Thanks igorpadykov again !

0 Kudos
Reply

964 Views
igorpadykov
NXP Employee
NXP Employee

Hi 龙

I am afraid there is no data for boot case, however seems it

will be the same as in AN4580 sect.3.3.1 MP3 Audio Playback

Best regards

igor

0 Kudos
Reply