why I can't find and download L3.0.35_12.09.01_GA_source ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why I can't find and download L3.0.35_12.09.01_GA_source ?

Jump to solution
880 Views
少村黃
Contributor I

Dear All :

I want to use CentOS 64  install ltib and build U-boot .

But I only find this document use CentOS

CentOS 6.3 64-bit Host Building i.MX6Q-SDB Linux L3.0.35_12.09.01.01_GA_Source

so I think ,if I want to use CentOS build code and I have to use L3.0.35_12.09.01?

Because I try to use L3.0.35_4.1.0_130816_source  code , it's can't work.

please give me some idea!!!

0 Kudos
1 Solution
676 Views
Yuri
NXP Employee
NXP Employee

  I think it would be better to use Ubuntu or Debian as host PC for 
i.MX6 Linux building, since this Linux branch mainly is used by BSP
designers.

Please refer to the next Community link for recent

recommendations about Linux host setup :

"i.MX Linux BSP Environment Setup"

https://community.freescale.com/docs/DOC-95042


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
677 Views
Yuri
NXP Employee
NXP Employee

  I think it would be better to use Ubuntu or Debian as host PC for 
i.MX6 Linux building, since this Linux branch mainly is used by BSP
designers.

Please refer to the next Community link for recent

recommendations about Linux host setup :

"i.MX Linux BSP Environment Setup"

https://community.freescale.com/docs/DOC-95042


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
676 Views
少村黃
Contributor I

Dear Yuri

     thanks your response

    

     I think, must change Ubuntu is the best result!

Best regards

0 Kudos