Hi all,
pls give any idea for below issue.
U-Boot 2009.08-dirty (Oct 20 2014 - 10:46:22)
CPU: Freescale i.MX6 family TO1.2 at 792 MHz
Temperature: 49 C, calibration data 0x5734d669
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 29333333Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]
Boot Device: SD
I2C: ready
DRAM: 1 GB
MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3
In: serial
Out: serial
Err: serial
i2c: I2C3 SDA is low, start i2c recovery...
I2C3 Recovery success
Net: got MAC address from IIM: 00:00:00:00:00:00
FEC0 [PRIME]
Hit any key to stop autoboot: 0
MX6Q SABRESD U-Boot > tftp uImage 0x10800000
FEC: Link is Up 796d
Using FEC0 device
TFTP from server 172.16.1.129; our IP address is 172.16.1.141
Filename '0x10800000'.
Load address: 0x0
Loading: *
TFTP error: 'File not found' (1)
Starting again
FEC: Link is Up 796d
Abort
MX6Q SABRESD U-Boot > tftp uImage
FEC: Link is Up 796d
Using FEC0 device
TFTP from server 172.16.1.129; our IP address is 172.16.1.141
Filename 'uImage'.
Load address: 0x10800000
Loading: #######T ##T ###############################T #########################
#########T T ######T #########T T ##############T ##T ###########################
###############T #################T #T ######T ##########################T
#####T #########T #######T ############################T #T T ###############
#######T ##T ###T ##T ##T #T ####T #####T ##T ########T #T T #########T ###T ###T #####T #T ####
done
Bytes transferred = 4709252 (47db84 hex)
MX6Q SABRESD U-Boot > bootm
## Booting kernel from Legacy Image at 10800000 ...
Image Name: Linux-3.0.35-06114-g3b96084
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 4709188 Bytes = 4.5 MB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Initializing cgroup subsys cpu
Linux version 3.0.35-06114-g3b96084 (umamahesh@sysadmin-Veriton-Series) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #1 SMP PREEMPT Mon Dec 2 10:05:50 IST 2013
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board
Memory policy: ECC disabled, Data cache writealloc
CPU identified as i.MX6Q, silicon rev 1.2
PERCPU: Embedded 7 pages/cpu @c12f5000 s6592 r8192 d13888 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 203744
Kernel command line: console=ttymxc0,115200 androidboot.console=ttymxc0 vmalloc=400M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60 video=mxcfb1:off video=mxcfb2:off fbmem=28M
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 591MB 212MB = 803MB total
Memory: 803232k/803232k available, 245344k reserved, 413568K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xfbe00000 - 0xffe00000 ( 64 MB)
vmalloc : 0xd9800000 - 0xf2000000 ( 392 MB)
lowmem : 0xc0000000 - 0xd9000000 ( 400 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc0045000 ( 244 kB)
.text : 0xc0045000 - 0xc08cacd4 (8728 kB)
.data : 0xc08cc000 - 0xc09639e0 ( 607 kB)
.bss : 0xc0963a04 - 0xc0aeb748 (1568 kB)
Preemptible hierarchical RCU implementation.
NR_IRQS:624
MXC GPIO hardware
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
arm_max_freq=1.2GHz
MXC_Early serial console at MMIO 0x2020000 (options '115200')
bootconsole [ttymxc0] enabled
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
Initializing cgroup subsys debug
Initializing cgroup subsys cpuacct
Initializing cgroup subsys freezer
CPU: Testing write buffer coherency: ok
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
CPU1: Booted secondary processor
CPU2: Booted secondary processor
CPU3: Booted secondary processor
Brought up 4 CPUs
SMP: Total of 4 processors activated (6324.22 BogoMIPS).
print_constraints: dummy:
NET: Registered protocol family 16
print_constraints: vddpu: 725 <--> 1300 mV at 700 mV fast normal
print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal
print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal
print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal
print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal
print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal
U-Boot 2009.08-dirty (Oct 20 2014 - 10:46:22)
CPU: Freescale i.MX6 family TO1.2 at 792 MHz
Temperature: 50 C, calibration data 0x5734d669
Regards
Anandaraj
Hi anandraj
these messages are not errors, hanging may be caused by wrong
image (for example not for this board), one can try official demos below
and boot from SD card
L3.10.17_1.0.0_IMX6QDLS_BUNDLE : Source Code Download Steps Documentation and Demo Images.
Best regards
igor
Hi igor
I am trying to port android kernel and root file system.
Best regards
Anandaraj
Hi igor
This is first time i am doing this kernel porting.so could you tell why it hanging and rebooted.
Regars
Anandaraj