Freescale i.MX6Q MX6-SabreSD hangup at "print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freescale i.MX6Q MX6-SabreSD hangup at "print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal"

2,602 Views
anandrajm
Contributor I

Hi all,

pls give any idea for below issue.

U-Boot 2009.08-dirty (Oct 20 2014 - 10:46:22)

CPU: Freescale i.MX6 family TO1.2 at 792 MHz

Temperature:   49 C, calibration data 0x5734d669

mx6q pll1: 792MHz

mx6q pll2: 528MHz

mx6q pll3: 480MHz

mx6q pll8: 50MHz

ipg clock     : 66000000Hz

ipg per clock : 66000000Hz

uart clock    : 80000000Hz

cspi clock    : 60000000Hz

ahb clock     : 132000000Hz

axi clock   : 264000000Hz

emi_slow clock: 29333333Hz

ddr clock     : 528000000Hz

usdhc1 clock  : 198000000Hz

usdhc2 clock  : 198000000Hz

usdhc3 clock  : 198000000Hz

usdhc4 clock  : 198000000Hz

nfc clock     : 24000000Hz

Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]

Boot Device: SD

I2C:   ready

DRAM:   1 GB

MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3

In:    serial

Out:   serial

Err:   serial

i2c: I2C3 SDA is low, start i2c recovery...

I2C3 Recovery success

Net:   got MAC address from IIM: 00:00:00:00:00:00

FEC0 [PRIME]

Hit any key to stop autoboot:  0

MX6Q SABRESD U-Boot > tftp uImage 0x10800000

FEC: Link is Up 796d

Using FEC0 device

TFTP from server 172.16.1.129; our IP address is 172.16.1.141

Filename '0x10800000'.

Load address: 0x0

Loading: *

TFTP error: 'File not found' (1)

Starting again

FEC: Link is Up 796d

Abort

MX6Q SABRESD U-Boot > tftp uImage

FEC: Link is Up 796d

Using FEC0 device

TFTP from server 172.16.1.129; our IP address is 172.16.1.141

Filename 'uImage'.

Load address: 0x10800000

Loading: #######T ##T ###############################T #########################

         #########T T ######T #########T T ##############T ##T ###########################

         ###############T #################T #T ######T ##########################T

         #####T #########T #######T ############################T #T T ###############

         #######T ##T ###T ##T ##T #T ####T #####T ##T ########T #T T #########T ###T ###T #####T #T ####

done

Bytes transferred = 4709252 (47db84 hex)

MX6Q SABRESD U-Boot > bootm

## Booting kernel from Legacy Image at 10800000 ...

   Image Name:   Linux-3.0.35-06114-g3b96084

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    4709188 Bytes =  4.5 MB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.

Initializing cgroup subsys cpu

Linux version 3.0.35-06114-g3b96084 (umamahesh@sysadmin-Veriton-Series) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #1 SMP PREEMPT Mon Dec 2 10:05:50 IST 2013

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board

Memory policy: ECC disabled, Data cache writealloc

CPU identified as i.MX6Q, silicon rev 1.2

PERCPU: Embedded 7 pages/cpu @c12f5000 s6592 r8192 d13888 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 203744

Kernel command line: console=ttymxc0,115200 androidboot.console=ttymxc0 vmalloc=400M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60 video=mxcfb1:off video=mxcfb2:off fbmem=28M

PID hash table entries: 2048 (order: 1, 8192 bytes)

Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)

Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)

Memory: 591MB 212MB = 803MB total

Memory: 803232k/803232k available, 245344k reserved, 413568K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    DMA     : 0xfbe00000 - 0xffe00000   (  64 MB)

    vmalloc : 0xd9800000 - 0xf2000000   ( 392 MB)

    lowmem  : 0xc0000000 - 0xd9000000   ( 400 MB)

    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

    modules : 0xbf000000 - 0xbfe00000   (  14 MB)

      .init : 0xc0008000 - 0xc0045000   ( 244 kB)

      .text : 0xc0045000 - 0xc08cacd4   (8728 kB)

      .data : 0xc08cc000 - 0xc09639e0   ( 607 kB)

       .bss : 0xc0963a04 - 0xc0aeb748   (1568 kB)

Preemptible hierarchical RCU implementation.

NR_IRQS:624

MXC GPIO hardware

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

arm_max_freq=1.2GHz

MXC_Early serial console at MMIO 0x2020000 (options '115200')

bootconsole [ttymxc0] enabled

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

Initializing cgroup subsys debug

Initializing cgroup subsys cpuacct

Initializing cgroup subsys freezer

CPU: Testing write buffer coherency: ok

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

CPU1: Booted secondary processor

CPU2: Booted secondary processor

CPU3: Booted secondary processor

Brought up 4 CPUs

SMP: Total of 4 processors activated (6324.22 BogoMIPS).

print_constraints: dummy:

NET: Registered protocol family 16

print_constraints: vddpu: 725 <--> 1300 mV at 700 mV fast normal

print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal

print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal

print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal

print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal

print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal

U-Boot 2009.08-dirty (Oct 20 2014 - 10:46:22)

CPU: Freescale i.MX6 family TO1.2 at 792 MHz

Temperature:   50 C, calibration data 0x5734d669

Regards

Anandaraj

Labels (4)
0 Kudos
7 Replies

2,039 Views
igorpadykov
NXP Employee
NXP Employee

Hi anandraj

these messages are not errors, hanging may be caused by wrong

image (for example not for this board), one can try official demos below

and boot from SD card

L3.10.17_1.0.0_IMX6QDLS_BUNDLE : Source Code Download Steps Documentation and Demo Images.

L3.0.35_4.1.0_DEMO_IMAGE_BSP

Best regards

igor

0 Kudos

2,039 Views
anandrajm
Contributor I

Hi igor

I am trying  to port android  kernel and root file system.

Best regards

Anandaraj

0 Kudos

2,039 Views
igorpadykov
NXP Employee
NXP Employee

these messages from linux regulator driver

/linux/drivers/regulator/core.c

~igor

0 Kudos

2,039 Views
anandrajm
Contributor I

Hi igor

This is first time i am doing this kernel porting.so could you tell why it hanging and rebooted.

Regars

Anandaraj

0 Kudos

2,039 Views
igorpadykov
NXP Employee
NXP Employee

Hi anandraj

seems this is due to errors, please refer to attached file with porting hints.

One can add printfs in code to find out where problem occurs.

~igor

0 Kudos

2,039 Views
anandrajm
Contributor I

Hi igor

I am trying the L3.0.35_4.1.0_DEMO_IMAGE_BSP ,its also hanging same place.

Regards

Anandraj

0 Kudos

2,039 Views
igorpadykov
NXP Employee
NXP Employee

Hi anandraj

please check memory

https://community.freescale.com/docs/DOC-96412

~igor

0 Kudos