Can anyone share benchmarking information for sustained speed on the Ethernet port on the K60? I'm interested in:
- With MQX/RTCS, another RT/OS, or without OS
- TCP, UDP, and/or raw Ethernet packets
Using MQX/RTCS (4.1 with H/W IP checksum support turned on) on a TCP socket I was able to sustain 30Mb/sec transfers. This is running K60 @ 100MHz doing dummy writes of 1460 bytes each to an RTCS send().
But I'm really trying to get a sense for what the underlying hardware is capable of without the software overhead.
Thanks,
PMT
Hi pmt,
Unfortunately I don’t have updated information but please check the below information per Freescale MQX 4.0.0 Release Notes:
<--
RTCS TCP/IP code has been updated and throughput has been improved.
o Measured by Freescale FNET fBench tool: TCP TX~11Mbps; TCP RX~5Mbps; UDP TX ~25Mbps; UDP RX~24Mbps tested with TWRK60D100@96Mhz board at default configuration.
-->
This is on K60DN512 96 MHz,
I hope this helps, have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------