MK20DN512VLQ10 with CW 10.4.
Connected to flash which needs CS asserted through the command, address (both writes), and the reading of the data. I don't see a way to do this with SPIMaster_LDD short of taking over CS as a GPIO and controlling it directly. Is this correct, or am I missing something?
hello Mark:
There are some issues with the PE SPI driver (not really bugs, but deficiencies). You can find workarounds and more details in the next thread from the Freescale community:
https://community.freescale.com/thread/307520
==================================
this answer is for you. if it helps, please click on "correct answer" button. thanks!
Best Regards,
ZhangJun