About supporting LVDS panel (side by side) by i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About supporting LVDS panel (side by side) by i.MX6DQ.

Jump to solution
1,529 Views
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

Refer to attached file.

Is it possible to support attached LVDS display (Side by Side type) by i.MX6DQ?

Best Regards,

Keita

Labels (4)
0 Kudos
Reply
1 Solution
1,367 Views
igorpadykov
NXP Employee
NXP Employee

It isn't possible to use as Hardware (device)

Best regards

chip

View solution in original post

0 Kudos
Reply
4 Replies
1,367 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

unfortunately "side by side" configuration is not supported.

Split configuration [where both LVDS channels are used ] supports even pixels for LVDS0 and odd for LVDS1.

There are no other options.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,367 Views
keitanagashima
Senior Contributor I

Dear chipexpert,

Thank you for your prompt reply.

>unfortunately "side by side" configuration is not supported.

Which reason for that it isn't possible to use.

a) It isn't possible to use as Hardware (device).

b) It isn't possible to use because not supported Software BSP.

c) Other [Ex, It isn't possible to synchronize.]

Best Regards,

Keita

0 Kudos
Reply
1,368 Views
igorpadykov
NXP Employee
NXP Employee

It isn't possible to use as Hardware (device)

Best regards

chip

0 Kudos
Reply
1,367 Views
keitanagashima
Senior Contributor I

Dear chipexpert,

OK.

Thank you very much.

Best Regards,

Keita

0 Kudos
Reply