It is critical to maintain the recommended footprint of a 10 mils pad with a 15 mil open solder mask for
ease of fanout. In this case, the solder paste is the same as the pad with 15 mil, which allows an air gap.
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear jamesbone,
Is the 10 mils equal to 0.1mm?
Where is a 10 mils pad you mentioned in the diagram I sent?
I have no idea about the 10 mils pad.
Best Regards,
Keita