Hi everyone,
I have been trying to get the temperature from the value of the temperature sensor channel of the MC9RS08KB2 microcontroller.
The problem that i have is that i can not find the "VTEMP25" and "m" values for calculate the temperature.
Someone can tell me where I can find these values?
Regards.
Hello,
One of our TIC engineer has given these values, though I don't have the weblink for the same.
Temp Sensor Slope:
−40°C– 25°C 1.646 mV/°C
25°C– 125°C 1.769 mV/°C
Temp Sensor Voltage:
VTEMP25 = 701.2 mV
This might help.
If this post helps you, kindly mark it as correct/helpful answer.
-Arpita