CodeWarrior 10.3.3 and Yocto running on the P1010RDB -- Registry Initialization File

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior 10.3.3 and Yocto running on the P1010RDB -- Registry Initialization File

489 Views
pslavick
Contributor I

I am working with CodeWarrior 10.3.3 and Yocto running on the P1010RDB.  I am looking for a header/source file within the CodeWarrior directory that initialized the registry and demonstrates writing to certain bits in a register. If anyone can point me in the right direction inside of the CodeWarrior directory or if anyone knows the name of any such file please let me know.  CodeWarrior is running on a Windows 7 machine, by the way.

Labels (1)
0 Kudos
Reply
1 Reply

366 Views
addiyi
NXP Employee
NXP Employee

Attached you can find an example of header/source file that initialized and config a register. Also, in {CodeWarrior_Install_Path}\PA\PA_Support\Initialization_Files\QorIQ_P1 you can find the config file for P1010RDB, and you can see how the registers are defined and set.

0 Kudos
Reply