Error message "Verifying Checksum ... Bad Data CRC" appears when uboot load linux kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error message "Verifying Checksum ... Bad Data CRC" appears when uboot load linux kernel

25,949 Views
eddyliu
Contributor I

Hi Guys,

I add initramfs(based on busy box) in linux kernel compiling. uImage becomes bigger than default(no initramfs support):

uImage.PNG.png

Error message generates in the process of downloading uboot and kernel image using Mfgtools:

Header 1

U-Boot 2009.08 (Aug 16 2013 - 15:02:51)

CPU: Freescale i.MX6 family TO1.1 at 792 MHz

Thermal sensor with ratio = 188

Temperature:   39 C, calibration data 0x5a34e87d

mx6q pll1: 792MHz

mx6q pll2: 528MHz

mx6q pll3: 480MHz

mx6q pll8: 50MHz

ipg clock     : 66000000Hz

ipg per clock : 66000000Hz

uart clock    : 80000000Hz

cspi clock    : 60000000Hz

ahb clock     : 132000000Hz

axi clock   : 198000000Hz

emi_slow clock: 99000000Hz

ddr clock     : 396000000Hz

usdhc1 clock  : 198000000Hz

usdhc2 clock  : 198000000Hz

usdhc3 clock  : 198000000Hz

usdhc4 clock  : 198000000Hz

nfc clock     : 24000000Hz

Board: i.MX6DL/Solo-SABRESD: unknown-board Board: 0x61011 [POR ]

Boot Device: MMC

I2C:   ready

DRAM:  512 MB

MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3

Using default environment

In:    serial

Out:   serial

Err:   serial

Net:   got MAC address from IIM: 00:00:00:00:00:00

FEC0 [PRIME]

Hit any key to stop autoboot:  0

## Booting kernel from Legacy Image at 10800000 ...

   Image Name:   Linux-3.0.35-2508-g54750ff

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    9181376 Bytes =  8.8 MB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... Bad Data CRC

ERROR: can't get kernel image!

MX6Solo SABRESD-MFG U-Boot >

uboot environment:

Header 1

MX6Solo SABRESD-MFG U-Boot > printenv

bootargs=console=ttymxc0,115200 rdinit=/linuxrc enable_wait_mode=off nosmp

bootcmd=bootm 0x10800000 0x10c00000

bootdelay=0

baudrate=115200

ipaddr=192.168.1.103

serverip=192.168.1.101

netmask=255.255.255.0

loadaddr=0x10800000

rd_loadaddr=(0x10800000 + 0x300000)

netdev=eth0

ethprime=FEC0

uboot=u-boot.bin

kernel=uImage

stdin=serial

stdout=serial

stderr=serial

ethact=FEC0

Environment size: 371/131068 bytes

I enlarged parameter rd_loadaddr, which is 10 times than before:

Header 1

MX6Solo SABRESD-MFG U-Boot > set rd_loadaddr (0x10800000+0x1E00000)

MX6Solo SABRESD-MFG U-Boot > printenv

bootargs=console=ttymxc0,115200 rdinit=/linuxrc enable_wait_mode=off nosmp

bootcmd=bootm 0x10800000 0x10c00000

bootdelay=0

baudrate=115200

ipaddr=192.168.1.103

serverip=192.168.1.101

netmask=255.255.255.0

loadaddr=0x10800000

netdev=eth0

ethprime=FEC0

uboot=u-boot.bin

kernel=uImage

stdin=serial

stdout=serial

stderr=serial

ethact=FEC0

rd_loadaddr=(0x10800000+0x1E00000)

Environment size: 370/131068 bytes

But still same error appears:

Header 1

MX6Solo SABRESD-MFG U-Boot > boot

## Booting kernel from Legacy Image at 10800000 ...

   Image Name:   Linux-3.0.35-2508-g54750ff

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    9181376 Bytes =  8.8 MB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... Bad Data CRC

ERROR: can't get kernel image!

Labels (2)
0 Kudos
Reply
5 Replies

12,436 Views
Yuri
NXP Employee
NXP Employee

  Two possible reasons for the issue :

- kernel image was not written to the same place (start # of block) as was read ;

- kernel image size is not set correctly. 

  Please check if kernel image size is correct  in U-Boot command "mmc read".

Parameter length  (say, 0x1800 for 3M kernel) should be greater or equal real

kernel size.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

12,436 Views
raghuchaitanya
Contributor I

Hello Muri,

   Iam facing the same issue with i.MX6 Sabrelite platform. Below are the environment variables that I have issued by interuupting the booting for the first time.

MX6Q SABRELITE U-Boot > setenv bootcmd 'run bootargs; mmc dev 1;mmc read ${loadaddr} 0x800 0x2000;bootm'
MX6Q SABRELITE U-Boot > setenv bootargs 'console=ttymxc0,115200 root=/dev/mmcblk0p1 rootwait rw video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi'
MX6Q SABRELITE U-Boot > saveenv
Saving Environment to SPI Flash...
Erasing SPI flash...Erasing SPI NOR flash 0xc0000 [0x2000 bytes]
..SUCCESS

Writing to SPI flash...Writing SPI NOR flash 0xc0000 [0x2000 bytes] <- ram 0x276009b8
SUCCESS

done
MX6Q SABRELITE U-Boot > reset
resetting ...


U-Boot 2009.08-00530-g1f7edab (Nov 08 2012 - 10:51:22)

CPU:   Freescale i.MX 6 family 0.0V at 792 MHz
Temperature:   36 C, calibration data 0x5b050d7d
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock     : 66000000Hz
ipg per clock : 66000000Hz
uart clock    : 80000000Hz
cspi clock    : 60000000Hz
ahb clock     : 132000000Hz
axi clock   : 264000000Hz
emi_slow clock: 29333333Hz
ddr clock     : 528000000Hz
usdhc1 clock  : 200000000Hz
usdhc2 clock  : 200000000Hz
usdhc3 clock  : 200000000Hz
usdhc4 clock  : 200000000Hz
nfc clock     : 24000000Hz
Board: MX6Q-SABRELITE:[ WDOG]
Boot Device: I2C
DRAM:   1 GB
MMC:   FSL_USDHC: 0,FSL_USDHC: 1
JEDEC ID: 0xbf:0x25:0x41
Reading SPI NOR flash 0xc0000 [0x2000 bytes] -> ram 0x276009b8
SUCCESS

In:    serial
Out:   serial
Err:   serial
Checking for recovery command file...
Card did not respond to voltage select!
** Bad partition 6 **
** Bad partition 6 **
Net:   got MAC address from IIM: 11:22:33:44:55:66
FEC0 [PRIME]
Hit any key to stop autoboot:  0
Unknown command 'rootwait' - try 'help'
mmc1 is current device

MMC read: dev # 1, block # 2048, count 8192 ... 8192 blocks read: OK
## Booting kernel from Legacy Image at 10800000 ...
   Image Name:   Linux-3.0.35-2310-gc27cb38
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    3686476 Bytes =  3.5 MB
   Load Address: 10008000
   Entry Point:  10008000
   Verifying Checksum ... Bad Data CRC
ERROR: can't get kernel image!
MX6Q SABRELITE U-Boot >

can you please let me know where Iam going wrong? I have used the below procedure to flash the microSD card.

[root@localhost Binaries]# ls
rootfs  rootfs.tgz  u-boot.bin  uImage
[root@localhost Binaries]# dd if=u-boot.bin of=/dev/sdb1 bs=512 && sync && sync
349+1 records in
349+1 records out
179040 bytes (179 kB) copied, 0.160394 s, 1.1 MB/s
[root@localhost Binaries]# dd if=uImage of=/dev/sdb bs=512 seek=2048 && sync && sync
7200+1 records in
7200+1 records out
3686540 bytes (3.7 MB) copied, 1.85114 s, 2.0 MB/s
[root@localhost Binaries]# cd rootfs/
[root@localhost rootfs]# fdisk -l

Disk /dev/sda: 500.1 GB, 500107862016 bytes, 976773168 sectors
Units = sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disk identifier: 0x8b7ac3f0

   Device Boot      Start         End      Blocks   Id  System
/dev/sda1   *        2048      206847      102400    7  HPFS/NTFS/exFAT
/dev/sda2          206848   209717247   104755200    7  HPFS/NTFS/exFAT
/dev/sda3       209717248   210126847      204800   83  Linux
/dev/sda4       210126848   976773167   383323160    5  Extended
/dev/sda5       524703744   629561343    52428800   83  Linux
/dev/sda6       629563392   663117823    16777216   82  Linux swap / Solaris
/dev/sda7       663119872   976771071   156825600   83  Linux
/dev/sda8       210130263   524698964   157284351   83  Linux

Partition table entries are not in disk order

Disk /dev/sdb: 3904 MB, 3904897024 bytes, 7626752 sectors
Units = sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disk identifier: 0x00000000

   Device Boot      Start         End      Blocks   Id  System
/dev/sdb1            8192     7626751     3809280    b  W95 FAT32
[root@localhost rootfs]# fdisk /dev/sdb
Welcome to fdisk (util-linux 2.22.2).

Changes will remain in memory only, until you decide to write them.
Be careful before using the write command.


Command (m for help): d
Selected partition 1
Partition 1 is deleted

Command (m for help): d
No partition is defined yet!

Command (m for help): u
Changing display/entry units to cylinders (DEPRECATED!)

Command (m for help): u
Changing display/entry units to sectors

Command (m for help): n
Partition type:
   p   primary (0 primary, 0 extended, 4 free)
   e   extended
Select (default p): p
Partition number (1-4, default 1): 1
First sector (2048-7626751, default 2048): 8192
Last sector, +sectors or +size{K,M,G} (8192-7626751, default 7626751): 
Using default value 7626751
Partition 1 of type Linux and of size 3.6 GiB is set

Command (m for help): d
Selected partition 1
Partition 1 is deleted

Command (m for help): d
No partition is defined yet!

Command (m for help): d
No partition is defined yet!

Command (m for help): n
Partition type:
   p   primary (0 primary, 0 extended, 4 free)
   e   extended
Select (default p): p
Partition number (1-4, default 1): 1
First sector (2048-7626751, default 2048): 8192
Last sector, +sectors or +size{K,M,G} (8192-7626751, default 7626751): 
Using default value 7626751
Partition 1 of type Linux and of size 3.6 GiB is set

Command (m for help): w
The partition table has been altered!

Calling ioctl() to re-read partition table.
Syncing disks.
[root@localhost rootfs]# mkfs.ext3 /dev/sdb1
mke2fs 1.42.5 (29-Jul-2012)
Filesystem label=
OS type: Linux
Block size=4096 (log=2)
Fragment size=4096 (log=2)
Stride=0 blocks, Stripe width=0 blocks
238080 inodes, 952320 blocks
47616 blocks (5.00%) reserved for the super user
First data block=0
Maximum filesystem blocks=977272832
30 block groups
32768 blocks per group, 32768 fragments per group
7936 inodes per group
Superblock backups stored on blocks: 
     32768, 98304, 163840, 229376, 294912, 819200, 884736

Allocating group tables: done                            
Writing inode tables: done                            
Creating journal (16384 blocks): done
Writing superblocks and filesystem accounting information: done 

[root@localhost rootfs]# mount /dev/sdb1 /mnt/
[root@localhost rootfs]# cp -r* /mnt/
cp: invalid option -- '*'
Try 'cp --help' for more information.
[root@localhost rootfs]# cp -r * /mnt/
[root@localhost rootfs]# umount /mnt 

0 Kudos
Reply

12,439 Views
Yuri
NXP Employee
NXP Employee

Looks like Kernel size is small.

Please try the following :

MX6Q SABRELITE U-Boot > setenv bootcmd 'run bootargs; mmc dev 1;mmc read ${loadaddr} 0x800 0x3000;bootm'

~Yuri.

0 Kudos
Reply

12,439 Views
YixingKong
Senior Contributor IV

Eddy

We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply

12,439 Views
YixingKong
Senior Contributor IV

Eddy

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply