Kinetis K61 POR flag bit in RCM_SRS0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K61 POR flag bit in RCM_SRS0

968 Views
GordyCarlson
NXP Employee
NXP Employee

1.  Is the POR reset bit in the RCM_SRS0 register only set on a VDD POR?  Are there any other instances that will set this bit?

2. If the VDD POR were to occur while the K61 is in VLLS2, will the chip wake up via a reset?

Background:

- Customer uses two MK61FN1M0CAA12's running in lockstep in their design.  They use an external osc divided down to a 50Mhz core and bus clock. and approx a 20Mhz Flexbus and Flash clock.

- They use one supply source of 1.8v to supply power to VDD and VBAT to both chips.

- The chip will boot up to full run mode, and after sensing inactivity will transition to VLPR mode.  Upon an interrupt or command the chip will transition back to RUN mode and handle the interrupt or command,

- If main power is removed the code will transition to K61 to VLLS2 mode.  There is a 1.8v "Hold Up Battery" to keep voltage to the chip when main power is removed.

- There are various low level wakeups enabled while the chips are in VLLS2 mode.   We have DRYICE enabled for Pin and Voltage tamper.

- We use the 32 byte VBAT ad SYSTEM registers to store data. If a POR happens we expect the data stored in these locations to be invalid.

KEY ASPECT:   On a POR we expect DRYICE to remove data in VBAT register only.  For this reason we use the POR bit in the RCM_SRS0 register to indicate that a VDD POR bas occurred. If we see that this bit is set we will initialize the VBAT and SYSTEM registers.   However we are seeing intermittent POP occurences, which impact our board's proper operation.

Labels (1)
0 Kudos
Reply
2 Replies

623 Views
zhaohuiliu
NXP Employee
NXP Employee

Hi,

How about the 1.8v "Hold Up Battery" drive capability? Have you checked the VDD input to MCU while you see the POR event? You know once MCU is wake up by any source, MCU will suck large current from VDD than VLLS2 mode, which may drop the VDD level. When i did some Kinetis chips validation and i used multimeter to check the current of VLLSx mode, i always put the multimeter in uA range. If i waked up MCU in that case, MCU would be in LVD reset, for the multimeter would have limited the current, which dropped the VDD to MCU.  Normal current for K61 may be around 50mA, Two MCU will use 100mA if they wake up at the same time. So please check the 1.8v drive capability, and RCM_SRS0[LVD] bit also. It may be a real POR for your case.

Hope this helpful

Thanks,

Sandy

623 Views
GordyCarlson
NXP Employee
NXP Employee

Yes,  you are in sync with us.  In parallel we have also been checking the performance of the voltage regulator.  We also suspect it may be the issue.   Confirming that the POR bit is only set by a VDD power on reset has helped us focus on a possible voltage fluctuation.   Thanks!

-Gordy

0 Kudos
Reply