Unused supplies on PF0100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unused supplies on PF0100

Jump to solution
941 Views
emil
Contributor III

Hello,

I've made a construction with iMX6 solo based on the Sabre SD development board. It looks like I'm not going to need some regulators from the PF0100, for instance VGEN1 and VGEN2. I assume their outputs should just be NC then? Also, this implies that I do not need to connect any supply to VIN1 (which powers VGEN1 and VGEN2). Is this correct? Can I just leave VIN1 unconnected and connect VIN2 and VIN3 only?

BR,

Emil

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
728 Views
Yuri
NXP Employee
NXP Employee

Please refer to Table 1 (MMPF0100 Pin Connection Guidelines) of AN4717

(Schematic Guidelines for the MMPF0100).

http://cache.freescale.com/files/analog/doc/app_note/AN4717.pdf

View solution in original post

0 Kudos
Reply
1 Reply
729 Views
Yuri
NXP Employee
NXP Employee

Please refer to Table 1 (MMPF0100 Pin Connection Guidelines) of AN4717

(Schematic Guidelines for the MMPF0100).

http://cache.freescale.com/files/analog/doc/app_note/AN4717.pdf

0 Kudos
Reply