Unused supplies on PF0100

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unused supplies on PF0100

ソリューションへジャンプ
760件の閲覧回数
emil
Contributor III

Hello,

I've made a construction with iMX6 solo based on the Sabre SD development board. It looks like I'm not going to need some regulators from the PF0100, for instance VGEN1 and VGEN2. I assume their outputs should just be NC then? Also, this implies that I do not need to connect any supply to VIN1 (which powers VGEN1 and VGEN2). Is this correct? Can I just leave VIN1 unconnected and connect VIN2 and VIN3 only?

BR,

Emil

ラベル(1)
タグ(3)
0 件の賞賛
1 解決策
547件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please refer to Table 1 (MMPF0100 Pin Connection Guidelines) of AN4717

(Schematic Guidelines for the MMPF0100).

http://cache.freescale.com/files/analog/doc/app_note/AN4717.pdf

元の投稿で解決策を見る

0 件の賞賛
1 返信
548件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please refer to Table 1 (MMPF0100 Pin Connection Guidelines) of AN4717

(Schematic Guidelines for the MMPF0100).

http://cache.freescale.com/files/analog/doc/app_note/AN4717.pdf

0 件の賞賛