Hi community,
I have a question about i.MX6 SSIx_STCR explanation in reference manual.
Please see chapter 61.9.7 in IMX6DQRM (Rev.1)
The explanation is lacking after "Finally, the interrupt can be enabled from within the".
And chapter 61.9.7 in IMX6SDLRM (Rev.1) and chapter 48.9.7 in IMX6SLRM (Rev.1) are lacking it, too.
Could you let me know the next explanation after that?
Best Regards,
Satoshi Shimoda
Solved! Go to Solution.
As for chapter 61.9.7 in IMX6DQRM (Rev.1) :
"Finally, the interrupt can be enabled from within the SSI."
As for chapter 61.9.7 in IMX6DQRM (Rev.1) :
"Finally, the interrupt can be enabled from within the SSI."