Could you let me know the lacked explanation about i.MX6 SSIx_STCR in reference manual?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could you let me know the lacked explanation about i.MX6 SSIx_STCR in reference manual?

Jump to solution
604 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 SSIx_STCR explanation in reference manual.

Please see chapter 61.9.7 in IMX6DQRM (Rev.1)

The explanation is lacking after "Finally, the interrupt can be enabled from within the".

And chapter 61.9.7 in IMX6SDLRM (Rev.1) and chapter 48.9.7 in IMX6SLRM (Rev.1) are lacking it, too.

Could you let me know the next explanation after that?

Best Regards,

Satoshi Shimoda

Labels (6)
Tags (1)
0 Kudos
1 Solution
510 Views
Yuri
NXP Employee
NXP Employee

  As for chapter 61.9.7 in IMX6DQRM (Rev.1) :

"Finally, the interrupt can be enabled from within the SSI."

View solution in original post

0 Kudos
1 Reply
511 Views
Yuri
NXP Employee
NXP Employee

  As for chapter 61.9.7 in IMX6DQRM (Rev.1) :

"Finally, the interrupt can be enabled from within the SSI."

0 Kudos