HDMI goes to sleep ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI goes to sleep ?

Jump to solution
2,718 Views
francoisrey
Contributor III

Hi,

I works on the demoboard of sabreLite of Element14. I have made a software to play some video on hdmi with gstreamer. After the system has boot (on linux 3.0 with busy box), my software send audio and video signal through HDMI and it works fine. But after about 8 minutes, there no more signal on the hdmi, I can always use the console through UART and my software still run. When I try to restart an avi file with an audio channel, it tell me that "asoc: can't open platform imx-hdmi-soc-audio.0".

It seems that after 8 minutes the system put HDMI in sleep mode, how can I avoid that ?

Labels (1)
1 Solution
1,990 Views
timothybean
Contributor IV

Hi,

You can try consoleblank=0 in your bootargs. That should keep the display from "going to sleep".

I had the same issue initially, after applying that it never blanks.

Tim

View solution in original post

2 Replies
1,991 Views
timothybean
Contributor IV

Hi,

You can try consoleblank=0 in your bootargs. That should keep the display from "going to sleep".

I had the same issue initially, after applying that it never blanks.

Tim

1,990 Views
francoisrey
Contributor III

Thanks a lot it works !

0 Kudos
Reply