mx53 can‘t boot wince7 from SD Card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

mx53 can‘t boot wince7 from SD Card

跳至解决方案
2,094 次查看
JackyHuang
Contributor III

Dear All:

Im a newer in wince7.

Now my company design a mx53 board base on the mx53smd reference board. 

We just reduce the ddr from 1G to 512M!

we can't boot the wince7 from SD Card, there is no print output to the UART.

however, we can boot android from SD Card succeed.

so, what can I do to make the wince7 boot from SD Card succeed?

Thanks advance!

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,848 次查看
king_jin
NXP Employee
NXP Employee

You need to configure the correct parameters for DDR memory in bootloader(hardware should help). Next you should define the IMGRAM512 macro in BSP manually.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,848 次查看
liaoaleon
Contributor I

I had the same problem,Can anyone tell me have configure it?!

0 项奖励
回复
1,848 次查看
JackyHuang
Contributor III

Thanks for your help,  I'll try it

0 项奖励
回复
1,849 次查看
king_jin
NXP Employee
NXP Employee

You need to configure the correct parameters for DDR memory in bootloader(hardware should help). Next you should define the IMGRAM512 macro in BSP manually.

0 项奖励
回复