I want to install the Flash File System (FFS) from NAND Flash File System patch for Freescale MQX™ RTOS 4.0.0 on the NANDFLASH chip on the TWR-K70.
I'm running the included example and I'm getting the following terminal output:
Shell (build: Mar 21 2013)
Copyright (c) 2008 Freescale Semiconductor;
shell>
shell> fsopen
Unable to open nandflash device.
You must run Repair command
shell> nandrepair
Repairing...
Repair successfully
shell> fsopen
NAND flash device was opened.
shell> dir
Error, file system not mounted
shell>
Has someone got an idea what might be wrong. Are there any jumper settings necessary?
Is it correct that ENABLE_NANDFLASH must be set to zero in the BSP like stated in the nandflash_wl_config.h?
Thank you for your help!
Solved! Go to Solution.
You need to add two lines (3 and 4 in the code snippet below) into _bsp_nandflash_io_init() in the BSP init_gpio.c, in order to specify divider of NFC clock:
SIM_SOPT2_REG(SIM_BASE_PTR) |= SIM_SOPT2_NFCSRC(0x00);
/* SIM_CLKDIV4: NFCDIV=7 */
SIM_CLKDIV4 &= 0x00FFFFFF; /* clear 8 most significant bits */
SIM_CLKDIV4 |= SIM_CLKDIV4_NFCDIV(7);
/* Enable clock gate to NFC module */
sim->SCGC3 |= SIM_SCGC3_NFC_MASK;
I tried that this works with PE Generated Code for the TWR-K70F120M BSP.
Hi,
I am using TWR-K60. and I am able to run example project. but when I restart and call fsopen, it says "NOT A DOS DISK! You must format to continue.". how can I solve this problem.
Also after formatting, it says "Free disk space: 10723328 bytes", although I have 2Gb nand flash.
Thank you...
Hi Okan,
Which version of MQX are you using? Check here Change size of FFS drive (MQX 4.0.1, TWR-K70)
-Daniel
Try "nanderasechip" command, as recommended by the MQXFFSUG Rev 1.1 on page 34.
Thank you for your answer.
I tried with "nanderasechip", but still the same problem:
Shell (build: Mar 21 2013)
Copyright (c) 2008 Freescale Semiconductor;
shell>
shell> nanderasechip
Erasing entire chip ...
Please use fsopen command to re-open NAND flash device.
shell> fsopen
Unable to open nandflash device.
You must run Repair command
shell> nandrepair
Repairing...
Repair successfully
shell> fsopen
NAND flash device was opened.
shell> dir
Error, file system not mounted
shell>
Can you tell me where I can find the MQXFFSUG document you are talking about? It is not in my FFS directory and I can find it nowhere else either.
Thanks!
in the /doc/ffs.
Have you tried nandlfash demo (without wear leveling layer) just to check the NFC driver works in your BSP setup ? /mqx/examples/nandflash/
For this demo you will need BSPCFG_ENABLE_NANDFLASH.
Sorry. I forgot to look in the most obvious place for the user guide.
I tried the basic nandflash example and got the following output (shortened):
MQX NAND Flash Example Application
==================================
NAND Flash device nandflash: opened
Obtaining NAND Flash organization data ...
ID: 0x0
Physical page size: 2048 bytes
Spare area size: 64 bytes
Block size: 131072 bytes
Number of blocks: 2048
Width: 16
Number of virtual pages: 524288
Virtual page size: 512 bytes
Block #0 is bad
(...)
Block #2047 is bad
Failed to get write buffer
Does this tell you something?
I added "block_size = block_size/8;" to nandflash_demo.c (line 250) as it is added for K60. Now I get:
MQX NAND Flash Example Application
==================================
NAND Flash device nandflash: opened
Obtaining NAND Flash organization data ...
ID: 0x0
Physical page size: 2048 bytes
Spare area size: 64 bytes
Block size: 131072 bytes
Number of blocks: 2048
Width: 16
Number of virtual pages: 524288
Virtual page size: 512 bytes
Block #0 is bad
(...)
Block #2047 is bad
Erasing block #0 failed.
Writing data to 32 virtual pages of block #0 ... Done
Reading data back from 32 virtual pages of block #0 ... Failed
Comparing data ... Compare failed
Still using Flexbus for TWR-LCD ? Some Flexbus signals are shared with NFC signals. Like PTB20 being NFC_DATA1 or FB_AD31. Try to remove the TWR-LCD from the tower.
I had the same idea and I already isolated the tower board from the rest of the hardware to avoid any interferences.
Actually I found the cause of the problem here in this unanswered question: nand_flash mqx demo doesn't work on K70
I removed "Sources" and the "Generated Code" directory from my BSP, recompiled it and now the NANDFLASH example works like a charm. I haven't tested FFS yet, but I guess that the problems there were caused by the same "bug".
Maybe someone should have a closer look why PE code interferes with NANDFLASH.
You need to add two lines (3 and 4 in the code snippet below) into _bsp_nandflash_io_init() in the BSP init_gpio.c, in order to specify divider of NFC clock:
SIM_SOPT2_REG(SIM_BASE_PTR) |= SIM_SOPT2_NFCSRC(0x00);
/* SIM_CLKDIV4: NFCDIV=7 */
SIM_CLKDIV4 &= 0x00FFFFFF; /* clear 8 most significant bits */
SIM_CLKDIV4 |= SIM_CLKDIV4_NFCDIV(7);
/* Enable clock gate to NFC module */
sim->SCGC3 |= SIM_SCGC3_NFC_MASK;
I tried that this works with PE Generated Code for the TWR-K70F120M BSP.
hi,
Is it a bug fix? Why did not it come out with the release 4.1.0 of MQX?
Thranks,
Rui Faria
freescale please fix this