Hello,
does anybody know if there is an eagle library for Kinetis K40 and K20 microcontroller??
Thanks,
Jose
Solved! Go to Solution.
I am not sure what are you looking for. but we have the Capture Symbol (orcad) and the Footprint (land pattern) Cadence Allegro(dra) for some of our MCU, you can find this information under the icon that is show when you search a part number. For instance, if you search the part number MK40DN512VMD10 on the ordenable part you will get the following result
and on this page just make click on the icon to get MK40DN512VMD10 Information
Where you can get information about the package, Environmental and Compliance etc
For different part number you just need to put the correct part number and follow the same process
I hope this will help you.
Regards
Vicente
Hello Jose,
did that answered your question? Please don't forget to keep us posted :smileywink:
Best regards,
Monica
Yes I solved the problem with this answer
Thanks
Jose
I am not sure what are you looking for. but we have the Capture Symbol (orcad) and the Footprint (land pattern) Cadence Allegro(dra) for some of our MCU, you can find this information under the icon that is show when you search a part number. For instance, if you search the part number MK40DN512VMD10 on the ordenable part you will get the following result
and on this page just make click on the icon to get MK40DN512VMD10 Information
Where you can get information about the package, Environmental and Compliance etc
For different part number you just need to put the correct part number and follow the same process
I hope this will help you.
Regards
Vicente
I followed your instruction and I found
| |
Product Summary Page |
General Information
Package Information
Environmental and Compliance Information
Manufacturing Information
Ordering Information
Product/Process Change Notice (PCN)
Operating Characteristics
Reliability Data Lookup
continue Package information
I got 98ASA00474D.pdf from the following link. may be I have been using TI's chip for a long time. I feel it is hard to find useful information for this chip, I couldn't even find a land pattern in PDF format, in user manual, or data sheet. if not for the cost issue, I would keep using TI MSP chip. I guess I have to create the layout symbol from the chip package. it is a pain in the neck.
thanks,
David
Package Information
Parameter | Value | |
Package Type and Termination Count | QFN 24 | |
Package Description and Mechanical Drawing | QFN MAP 24 4*4*1 P0.5 | |
Device Weight(g) | .01580 | |
Package Length (nominal)(mm) | 4.000 | |
Package Width (nominal)(mm) | 4.000 | |
Package Thickness (nominal)(mm) | 1.000 | |
Tape & Reel | No |