Hello
I've just found the expert programmer mode and i'm running it
But without the expert programmer mode i had :
The two LED on my BDM are lighted.
So the BLUE one implies my bdm interface is powering and running, and the yellow that target power has been detected.
But when i click on debug, it opens the window "true time simulator & real time debugger" and a window entitled "ICD Connection Manager".
When i try to click on Connect on the window "ICD...", a new window "Erase and Program Flash" is displayed.
If i click on connect, the window "CPROGHCS08 programmer" is displayed, and the problem is that it runs forever after the command "EM"...
Message Edited by jbulysse1994 on
2007-07-09 09:22 AM