I would like export the "Generated_code" to my existing CW project, I can't find the
source code of the low level functions. The compiler will fail.
For example, in the UART3 component, there is function
LDD_TDeviceData* CMD_Uart3_Init(LDD_TUserData *UserDataPtr),
inside this function there is low level function
UART_PDD_SetBaudRate(UART3_BASE_PTR, 11U); /* Set the baud rate register. */
I can't find its source code, the compiler will fail on
Undefined : "UART_PDD_SetBaudRate".
Where is the low level source code?
Regards
Samuel
Solved! Go to Solution.
Hello,
the PDD macros are stored under the following path:
{YOUR INSTALLATION}\MCU\ProcessorExpert\lib\Kinetis\pdd\inc\
Details also in this thread:
Missing #include "GPIO_PDD.h" from Generated Code
best regards
Vojtech Filip
Processor Expert Support Team
Hello,
the PDD macros are stored under the following path:
{YOUR INSTALLATION}\MCU\ProcessorExpert\lib\Kinetis\pdd\inc\
Details also in this thread:
Missing #include "GPIO_PDD.h" from Generated Code
best regards
Vojtech Filip
Processor Expert Support Team