Hello,
i've got a problem with chip mpxy8300. I created blank project in codewarrior and try to set port:
#include <hidef.h> /* for EnableInterrupts macro */
#include "derivative.h" /* include peripheral declarations */
void main(void) {
PTADD=0x07;
PTAD=0x07;
for(;;) {
// __RESET_WATCHDOG(); /* feeds the dog */
} /* loop forever */
/* please make sure that you never leave main */
}
this code doesn't work. When i'm debugging it seems that uC don't go inside main function.
Does anybody know what i'm doing wrong.
Mirek
Thank's for your replies. Maybe it's a bug somewhere, i'm not so good programmer, can anybody try to find bug or help in other ways.
Regards
Mirek
/******************************************************************************
FILE : start08.c
PURPOSE : 68HC08 standard startup code
LANGUAGE : ANSI-C / INLINE ASSEMBLER
----------------------------------------------------------------------------
HISTORY
22 oct 93 Created.
04/17/97 Also C++ constructors called in Init().
******************************************************************************/
/**********************************************************************/
/* NOTE: */
/* This version of the startup code assumes that main */
/* does never return (saving the 2 byte return address of _Startup on */
/* the stack). */
/**********************************************************************/
#define __NO_FLAGS_OFFSET /* we do not need the flags field in the startup data descriptor */
#define __NO_MAIN_OFFSET /* we do not need the main field in the startup data descriptor */
#include <start08.h>
#ifdef __cplusplus
#define __EXTERN_C extern "C"
#else
#define __EXTERN_C
#endif
__EXTERN_C extern void main(void); /* prototype of main function */
#include "non_bank.sgm"
/***************************************************************************/
/* Macros to control how the startup code handles the COP: */
/* #define _DO_FEED_COP_ : do feed the COP */
/* Without defining any of these, the startup code does NOT handle the COP */
/***************************************************************************/
/* __ONLY_INIT_SP define: */
/* This define selects an shorter version of the startup code */
/* which only loads the stack pointer and directly afterwards calls */
/* main. This version does however NOT initialize global variables */
/* (so this version is not ANSI compliant!). */
/***************************************************************************/
#if defined(_DO_FEED_COP_)
#define __FEED_COP_IN_HLI() } _FEED_COP(); __asm {
#else
#define __FEED_COP_IN_HLI() /* do nothing */
#endif
#ifndef __ONLY_INIT_SP
#pragma DATA_SEG FAR _STARTUP
struct _tagStartup _startupData; /* read-only:
_startupData is allocated in ROM and
initialized by the linker */
#pragma MESSAGE DISABLE C20001 /* Warning C20001: Different value of stack pointer depending on control-flow */
/* the function _COPY_L releases some bytes from the stack internally */
#if defined(__OPTIMIZE_FOR_SIZE__) || defined(_DO_FEED_COP_)
#pragma NO_ENTRY
#pragma NO_EXIT
#pragma NO_FRAME
/*lint -esym(528, loadByte) inhibit warning about unreferenced loadByte function */
static void near loadByte(void) {
asm {
PSHH
PSHX
#ifdef __HCS08__
LDHX 5,SP
LDA 0,X
AIX #1
STHX 5,SP
#else
LDA 5,SP
PSHA
LDX 7,SP
PULH
LDA 0,X
AIX #1
STX 6,SP
PSHH
PULX
STX 5,SP
#endif
PULX
PULH
RTS
}
}
#endif /* defined(__OPTIMIZE_FOR_SIZE__) || defined(_DO_FEED_COP_) */
#ifdef __cplusplus
static void Call_Constructors(void) {
int i;
#ifdef __ELF_OBJECT_FILE_FORMAT__
i = (int)(_startupData.nofInitBodies - 1);
while (i >= 0) {
(&_startupData.initBodies->initFunc)[i](); /* call C++ constructors */
i--;
}
#else /* __ELF_OBJECT_FILE_FORMAT__ */
/* HIWARE object file format */
if (_startupData.mInits != NULL) {
_PFunc *fktPtr;
fktPtr = _startupData.mInits;
while(*fktPtr != NULL) {
(**fktPtr)(); /* call constructor */
fktPtr++;
}
}
#endif /* __ELF_OBJECT_FILE_FORMAT__ */
}
#endif
/*lint -esym(752,_COPY_L) inhibit message on function declared, but not used (it is used in HLI) */
__EXTERN_C extern void _COPY_L(void);
/* DESC: copy very large structures (>= 256 bytes) in 16-bit address space (stack incl.)
IN: TOS count, TOS(2) @dest, H:X @src
OUT:
WRITTEN: X,H */
#ifdef __ELF_OBJECT_FILE_FORMAT__
#define toCopyDownBegOffs 0
#else
#define toCopyDownBegOffs 2 /* for the hiware format, the toCopyDownBeg field is a long. Because the HC08 is big endian, we have to use an offset of 2 */
#endif
static void Init(void) {
/* purpose: 1) zero out RAM-areas where data is allocated
2) init run-time data
3) copy initialization data from ROM to RAM
*/
/*lint -esym(529,p,i) inhibit warning about symbols not used: it is used in HLI below */
int i;
int *far p;
asm {
ZeroOut:
LDA _startupData.nofZeroOuts:1 ; // nofZeroOuts
INCA
STA i:1 ; // i is counter for number of zero outs
LDA _startupData.nofZeroOuts:0 ; // nofZeroOuts
INCA
STA i:0
LDHX _startupData.pZeroOut ; // *pZeroOut
BRA Zero_5
Zero_3:
; // CLR i:1 is already 0
Zero_4:
; // { HX == _pZeroOut }
PSHX
PSHH
; // { nof bytes in (int)2,X }
; // { address in (int)0,X }
LDA 0,X
PSHA
LDA 2,X
INCA
STA p ; // p:0 is used for high byte of byte counter
LDA 3,X
LDX 1,X
PULH
INCA
BRA Zero_0
Zero_1:
; // CLRA A is already 0, so we do not have to clear it
Zero_2:
CLR 0,X
AIX #1
__FEED_COP_IN_HLI() ; // it's necessary to feed the COP in the inner loop for the fast COP timeout of some derivatives
Zero_0:
DBNZA Zero_2
Zero_6:
DBNZ p, Zero_1
PULH
PULX ; // restore *pZeroOut
AIX #4 ; // advance *pZeroOut
Zero_5:
DBNZ i:1, Zero_4
DBNZ i:0, Zero_3
CopyDown:
}
/* copy down */
/* _startupData.toCopyDownBeg ---> {nof(16) dstAddr(16) {bytes(8)}^nof} Zero(16) */
#if defined(__OPTIMIZE_FOR_SIZE__) || defined(_DO_FEED_COP_) /* for now: only -os version supports _DO_FEED_COP_ */
asm {
#ifdef __HCS08__
LDHX _startupData.toCopyDownBeg:toCopyDownBegOffs
PSHX
PSHH
#else
LDA _startupData.toCopyDownBeg:(1+toCopyDownBegOffs)
PSHA
LDA _startupData.toCopyDownBeg:(0+toCopyDownBegOffs)
PSHA
#endif
Loop0:
JSR loadByte ; // load high byte counter
TAX ; // save for compare
INCA
STA i
JSR loadByte ; // load low byte counter
INCA
STA i:1
DECA
BNE notfinished
CBEQX #0, finished
notfinished:
JSR loadByte ; // load high byte ptr
PSHA
PULH
JSR loadByte ; // load low byte ptr
TAX ; // HX is now destination pointer
BRA Loop1
Loop3:
Loop2:
__FEED_COP_IN_HLI()
JSR loadByte ; // load data byte
STA 0,X
AIX #1
Loop1:
DBNZ i:1, Loop2
DBNZ i:0, Loop3
BRA Loop0
finished:
AIS #2
}
#else /*defined(__OPTIMIZE_FOR_SIZE__) || defined(_DO_FEED_COP_) */
/* time optimized asm version. */
asm {
#ifdef __HCS08__
LDHX _startupData.toCopyDownBeg:toCopyDownBegOffs
#else
LDX _startupData.toCopyDownBeg:(0+toCopyDownBegOffs)
PSHX
PULH
LDX _startupData.toCopyDownBeg:(1+toCopyDownBegOffs)
#endif
next:
LDA 0,X ; // list is terminated by 2 zero bytes
ORA 1,X
BEQ copydone
PSHX ; // store current position
PSHH
LDA 3,X ; // psh dest low
PSHA
LDA 2,X ; // psh dest high
PSHA
LDA 1,X ; // psh cnt low
PSHA
LDA 0,X ; // psh cnt high
PSHA
AIX #4
JSR _COPY_L ; // copy one block
PULH
PULX
TXA
ADD 1,X ; // add low
PSHA
PSHH
PULA
ADC 0,X ; // add high
PSHA
PULH
PULX
AIX #4
BRA next
copydone:
}
#endif /* defined(__OPTIMIZE_FOR_SIZE__) || defined(_DO_FEED_COP_) */
/* FuncInits: for C++, this are the global constructors */
#ifdef __cplusplus
Call_Constructors();
#endif /* __cplusplus */
/* implement ROM libraries initialization here (see startup.c) */
}
#endif /* __ONLY_INIT_SP */
#pragma NO_EXIT
__EXTERN_C void _Startup(void) {
/* set the reset vector to _Startup in the linker parameter file (*.prm):
'VECTOR 0 _Startup'
purpose: 1) initialize the stack
2) initialize run-time, ...
initialize the RAM, copy down init data, etc (Init)
3) call main;
called from: _PRESTART-code generated by the Linker
*/
INIT_SP_FROM_STARTUP_DESC();
#ifndef __ONLY_INIT_SP
Init();
#endif
#ifndef __BANKED__
__asm JMP main; /* with a C style main(); we would push the return address on the stack wasting 2 RAM bytes */
#else
__asm CALL main;
#endif
}
Maybe there is a bug in basic project suggested by Freescale.
Try to stop the debugger at "Program Entry Point" instead of "User Specified: main" and go ahedd step by step to search for the problem.
I am using M5208EVB with Freescale demo example and It can't go to main because there is a bug in initialize_hardware() that jump at start again creating an infinite loop.
Regards
Maurizio
Hello,
that sounds like indeed the controller has performed a reset.
Multiple possible reasons:
- watchdog: is the watchdog disabled?
- power supply: I have seen cases were an unstable power supply resets the chip.
- clock settings: if the problem happens during (wrong) clock initialization, the chip might get a wrong frequency and resets.
Hope this helps,
Erich