Here's the whole post:
https://plus.google.com/u/0/104422661029399872488/posts/3VMp4uQgpNT
Binaries and instructions are located here:
https://android-build.linaro.org/builds/~linaro-android/staging-imx53-11.12-release/#build=1
Test results at:
https://docs.google.com/a/linaro.org/spreadsheet/ccc?key=0AkxwyUNxNaAadHlNN1hZZERMbThtaTBlSkZwVDRYdG...
Instructions to build for a similar board (snowball) that should work with a small modification for the iMX53:
http://www.linaro.org/linaro-blog/2011/11/24/compiling-the-snowball-ics-build-from-scratch/
Enjoy!
Does this work with the imx53 qsb Start-R boards? I have been looking for a working version...
I have Gingerbread working on my machine with prebuilt images but would be nice to use ICS or even maybe Jelly Bean if anyone has that working yet...
Rodney
Oh! If you're confused I'm not doing my job right :)
Here's a set of instructions that should work:
mkdir bin
export PATH=$PWD/bin:$PATH
curl https://dl-ssl.google.com/dl/googlesource/git-repo/repo > bin/repo
chmod a+x bin/repo
mkdir imx53_ics
cd imx53_ics
repo init -u git://android.git.linaro.org/platform/manifest.git -b linaro-android-11.12-release -m staging-iMX53.xml
repo sync
make TARGET_PRODUCT=iMX53 TARGET_TOOLS_PREFIX=./prebuilt/linux-x86/toolchain/arm-linux-androideabi-4.4.x/bin/arm-linux-androideabi- -j8 systemtarball userdatatarball boottarball
bzr branch lp:linaro-image-tools
# insert SD card
./linaro-image-tools/linaro-android-media-create --mmc /dev/sdc --dev snowball_sd --system /mnt/user/0_pfefferz/ics/snowball_ics/system.tar.bz2 --userdata /mnt/user/0_pfefferz/ics/snowball_ics/userdata.tar.bz2 --boot /mnt/user/0_pfefferz/ics/snowball_ics/boot.tar.bz2
Dear sir ,
could you please tell me which version of GCC i have to use to build above source.
thanks,
muthe
I always get confused when donwloading source code from Linaro git tree.
At this moment, I'm syncing:
./repo init -u git://android.git.linaro.org/platform/manifest.git -b linaro_android_4.0.1
following this page:
https://wiki.linaro.org/Platform/Android/BuildSource
I hope it works