COM Port is not working when I connect my board in this way
I am using minicom, all the necessary drivers have been installed.
When I use Serial Cable I connect with minicom configured like this
When I use USB i use Serial Device as /dev/ttyUSB0 .
When I use a USB to Serial Connector, the board is then working fine, I mean I am able to communicate with my board.
The serial cable and COM Port if used individually are working fine.
Any idea about this problem?
Regards :: Krishna Pavan
Hi,
As early mentioned I have been checking the DB9 connector.
Even the statserial software could show the same.
Which means that the COM Port is not receiving any data that is transmitted to it.
Here are the pics of the Stat Serial
I just connected the board, Now the booting sequence has been initiated after Power Up
Now I need to enter the log-in that is by default root
Now that stats are
Any Infererences?
Have any one faced the problem with the COM Ports on the board/PC. Regards :: Krishna Pavan
The loop back test using gtkterm/minicom did not give me any result.
Is there an error within the board or is the error with my PC?