HCS08 TIM simulation problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HCS08 TIM simulation problem

Jump to solution
2,373 Views
joerg
Contributor II
Hi
I try to simulate the output compare function for TIM1 of GB32/60, RC8 and QD4 MPUs.
But in the simulator the TIM does not trigger an interrupt. If i connect a MPU with the BDM it works just fine. The simulation of a TOF interrupt works in the full chip simulation. Is this a known problem (i noticed this behavior for CW3.1, CW3.2, CW5.0 and CW5.1!!)

Thanks Joerg

Message Edited by joerg on 2007-01-0112:30 PM

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
807 Views
CrasyCat
Specialist III
Hello
 
You need to submit a service request  for that.
This is an issue in P&E simulation module.  You can log that defect either with Freescale support or
directly with P&E.
 
To log the issue with Freescale please go to following URL:
and click on "Submit a service request"
 
To log the issue with P&E use following URL:
 
Note that Freescale support personal will anyway have to log that with P&E.
 
CrasyCat

View solution in original post

0 Kudos
Reply
3 Replies
808 Views
CrasyCat
Specialist III
Hello
 
You need to submit a service request  for that.
This is an issue in P&E simulation module.  You can log that defect either with Freescale support or
directly with P&E.
 
To log the issue with Freescale please go to following URL:
and click on "Submit a service request"
 
To log the issue with P&E use following URL:
 
Note that Freescale support personal will anyway have to log that with P&E.
 
CrasyCat
0 Kudos
Reply
807 Views
joerg
Contributor II
Thanks CrazyCat
i have put the service request on the freescale support page:

ID: 1-335781881

Saluti Joerg
0 Kudos
Reply
807 Views
Phoenix
Contributor III
This bug will be fixed in v5.2 update patch. It should be released at the end of January.
0 Kudos
Reply